(Read-Write) Set and query preamplifier state. Available with Option 235. |
|
Relevant Modes |
IQA |
Parameters |
|
<boolean> |
Preamp AUTO ON | OFF state. Choose from: O or OFF - AUTO Preamp OFF 1 or ON - AUTO Preamp ON When Auto is enabled, the preamp setting is coupled to the RF attenuation and to the reference level. When the reference level reaches a certain value, the preamp is turned on and PA is shown to the left of the graticules on the display. |
Examples |
POW:GAIN:AUTO 0 POW:GAIN:AUTO OFF |
Query Syntax |
:POW:GAIN:AUTO? |
Return Type |
Boolean |
Default |
OFF (0) |
Last Modified:
22oct2017 |
Added IQA mode (10.1x) |