|
(Read-Write) Set and query the channel number that appears at the stop (right edge) of the current channel measurement. First select a Radio Standard [:SENSe]:RADio:STANdard then activate the channel frequency-drive commands by changing [:SENSe]:RADio:TEUNit to CHAN. |
|
|
Relevant Modes |
SA |
|
Parameters |
|
|
<num> |
Stop channel number. The range of valid channel numbers depends on the current radio standard. If a channel number outside the acceptable range is entered, the channel will be set to the closest valid channel number. |
|
Examples |
RAD:CHAN:STOP 10 |
|
Query Syntax |
[:SENSe]:RADio:CHANnel:STOP? |
|
Return Type |
Numeric |
|
Default |
-1 (Start and Stop channels not activated) |