|
(Read-Write) Set and query the location of the Time or Delta marker, used with Waterfall and Spectrogram displays (Interference Analyzer 0pt 236). Use [:SENSe]:SPECtrogram:TMARker:STATe to enable the Time or Delta marker. Spectrogram displays the most recent record at the top of the screen. Waterfall displays the most recent record at the bottom. There is currently no command to read the Time that is displayed on the screen. |
|
|
Relevant Modes |
SA |
|
Parameters |
|
|
<num> |
Time or Delta marker location. Enter a value between 0 (bottom of screen) and the maximum number of records visible on the screen. The max number depends on the Waterfall view and Spectrogram Angle settings. |
|
Examples |
SPEC:TMAR:VAL 10 |
|
Query Syntax |
[:SENSe]:SPECtrogram:TMARker:VALue? |
|
Return Type |
Numeric |
|
Default |
0 |
Last Modified:
|
17-Aug-2012 |
Edited for both marker types |