[:SENSe]:SPECtrogram:TPDivision

(Read-Write) Set and query the Time per division of the Spectrogram trace graph window.

Relevant Modes

RTSA

Parameters

 

<num>

Per division time in seconds (0.0005 seconds to 10 seconds. Default = 100 ms).

Examples

SPEC:TPD 1e-3

SPEC:TPD 5

Query Syntax

[:SENSe]:TIME:PDIVision?

Return Type

Numeric

Default

1.000E-01


Last Modified:

19-sep-2016

New RTSA mode command (A.09.50)