|
(Read-Write) Set and query the direction in which the receivers are swept. |
|
|
Relevant Modes |
|
|
Parameters |
|
|
<value> |
Choose from the following: FORWard - Used for systems for which the output frequency is Offs + Src. The output frequency of the DUT and the receiver sweeps in the same direction as the source. REVerse - Used for systems for which the output frequency is Offs - Src. The output frequency of the DUT and the receiver sweeps in reverse direction as compared to the source. |
|
Examples |
SWE:RX REV |
|
Query Syntax |
[:SENSe]:SWEep:RX? |
|
Return Type |
Character |
|
Default |
FORWard |
Last modified:
|
19-Mar-2014 |
New command (A.07.50) |