|
(Read-Write) Set and query the resolution mode for the TDR measurement. This is the TDR Sweep setting in the FieldFox UI. |
|
|
Relevant Modes |
|
|
Parameters |
|
|
<num> |
Choose from: AUTO - Low pass frequency settings are calculated based on the current number of points. The Stop Frequency and Resolution settings can be changed to any value.
CABLe - Provides a higher resolution measurement or when under-sampling is suspected. The Stop Frequency is limited to 500 MHz maximum. The Resolution is fixed to 1601. |
|
Examples |
SWE:TDR:RES AUTO |
|
Query Syntax |
[:SENSe]:SWEep:TDR:RES? |
|
Return Type |
Character |
|
Default |
Auto |
Last Modified:
|
20-Jan-2015 |
New command (8.00) |