[:SENSe]:FREQuency:LO <num>

(Read-Write) Set and query the DUT LO frequency.

Note: The DUT LO frequency is only relevant for frequency converting DUTs (i.e., downconverter, upconverter, and multi-stage converter).

Relevant Modes

NF

Parameters

 

<numeric>

LO frequency in Hz. Choose a number between the minimum and maximum frequency of the FieldFox.

This command will accept MIN and MAX as arguments.

Examples

FREQ:LO 10E6

FREQ:LO MAX

Query Syntax

[:SENSe]:FREQuency:LO?

Return Type

Numeric

Default

--


Last Modified:

01-june-2018

Added Opt. 356 NF(10.3)