|
(Read-Write) Set and query the NREV frequency mode for the component carrier (CHANnel | FREQuency). |
|
|
Relevant Modes |
|
|
Couplings |
This setting is associated with the currently selected Component Carrier (CC). When Freq is selected, the frequency settings are set directly and when Chan is selected, the frequency settings are set through the channel table settings. |
|
Parameters |
|
|
<n> |
Choose from 1 to 5. Default is 1 (CC0). |
|
<char> |
Choices: CHANnel: Channel and Band are based on the component carrier in the FieldFox. Center frequency is coupled to the channel and band choices. FREQuency: Center frequency is entered independently. If FreqMode = Channel, center frequency value is based on band and channel in target carrier. |
|
Examples |
NREV:CCAR2:MODE CHAN NREV:CCAR2:MODE FREQ |
|
Query Syntax |
NREV:CCAR<n>:MODE? |
|
Return Type |
character |
|
Default |
numeric =1 (CC0), string = FREQ |
Last Modified:
|
15apr2020 |
A.12.00 New command |