[:SENse]:NREVm:CCARier<n>:FREQuency:CENTer <num>

(Read-Write) Set and query the component carrier center frequency.

Relevant Modes

5G NR EVM Conducted

Parameters

 

<n>

Component carrier (CC) number. If unspecified, value is set to 1 (CC0).

n = 1 | 2 | 3 | 4 | 5 (Up to five component carriers can be measured at one time.)

<num/char>

Carrier center frequency value in Hz.

MAXimum (Hz): Dynamic. Varies with the FieldFox model.

MINimum: 0 Hz

This command accept Default, MINimum and MAXimum as arguments.

Examples

NREV:CCAR5:FREQ:CENT 2e9

NREV:CCAR3:FREQ:CENT 10000

Query Syntax

NREV:CCAR<n>:FREQ:CENT?

Return Type

numeric

Default

1000000000


Last Modified:

12dec2019

New command