Note: This command was previously named [:SENSe]:ISOurce:ENABle. That syntax still work, but the new syntax should be used for new development. (Read-Write) Set and query the Independent source state. |
|
Relevant Modes |
SA |
Parameters |
|
<boolean> |
Independent source state. Choose from: ON (1) - Independent source ON OFF (0) - Independent source OFF |
Examples |
SOUR:ENAB 1 |
Query Syntax |
SOURce:ENABle? |
Return Type |
Boolean |
Default |
OFF |
Last Modified:
25-Mar-2014 |
Changed name |
20-Oct-2010 |
New command (5.30) |