(Read-Write) Set and query the frequency span of the measurement. Also send SOURce:FREQuency:CENTer |
|
Relevant Modes |
FOPS (Opt 208) |
Parameters |
|
<value> |
Frequency span in Hz. The frequency limits for the measurement are determined by the limits of both the FieldFox and the power sensor.
|
Examples |
SOUR:FREQ:SPAN .5e9 |
Query Syntax |
SOURce:FREQuency:SPAN? |
Return Type |
Numeric |
Default |
10 MHz |
Last modified:
19-Mar-2014 |
New command (A.07.50) |