|
(Read-Write) Set and query the stop frequency of the measurement. Also send SOURce:FREQuency:STARt |
|
|
Relevant Modes |
FOPS (Opt 208) |
|
Parameters |
|
|
<value> |
Stop frequency in Hz. The frequency limits for the measurement are determined by the limits of both the FieldFox and the power sensor.
|
|
Examples |
SOUR:FREQ:STOP 1.5e9 |
|
Query Syntax |
SOURce:FREQuency:STOP? |
|
Return Type |
Numeric |
|
Default |
55 MHz |
Last modified:
|
19-Mar-2014 |
New command (A.07.50) |