(Read-Write) Set and query the source power level. This command sets SOURce:POWer:ALC[:MODE] to MANual.
|
|
Relevant Modes |
CAT, NA, VVM, Power Meter |
Parameters |
|
<num> |
Source power/attenuator level.
This command also supports sending MIN and MAX power levels as arguments:
|
Examples |
SOUR:POW -10 Source:power max |
Query Syntax |
:SOURce:POWer? |
Return Type |
Numeric |
Default |
0 |
Last modified:
1-Nov-2013 |
Added Power Meter |
3-Apr-2013 |
Major edits (LH) |
15-Aug-2012 |
Added link to ALC mode |
17-Jul-2012 |
Added all other models (A.06.00) |
1-Feb-2011 |
Fixed and reworded to emphasize negative power levels. |