|
(Read-Write) Set or query the lan1 adapter on or off. lan1 corresponds to the 10 G SFP+ Ethernet port. Note: This command applies to FieldFox D-series (Fluyt) models and above. |
|
|
Relevant Modes |
ALL |
|
Parameters |
|
|
<string> |
Choose from: ON - Enable lan1 adapter. OFF - Disable lan1 adapter. |
|
Examples |
:SYST:COMM:LAN:ACT ON */Enable the lan1 adapter |
|
Query Syntax |
:SYST:COMM:LAN:ACT? |
|
Return Type |
string |
|
Default |
OFF |
Last modified:
|
25Feb2026 |
New command for D-series (D.14.04) and above. |