(Read-Write) Set and query the minimum saturated power allowed, before a satellite's power is used in the average power computation. |
|
Relevant Modes |
All modes |
Parameters |
|
<numeric> |
Choose from: 0 to 100 minimum C/no This command accepts MIN and MAX to set the minimum power required. |
Examples |
SYST:GPS:AVER:MINP 27 'sets the minimum satellite power required, before average power computation to 27 dB SYST:GPS:AVER:MINP MAX 'sets the satellite power required to maximum, before average power computation |
Query Syntax |
SYSTem:GPS:AVERage:MINP? |
Return Type |
numeric |
Default |
1 |
Last modified:
01nov2019 |
Added for PAA Mode |
20-Jul-2010 |
New command (A.05.33) |