(Read-Write) Set and query the top (most power) number of satellites to be displayed in the C/No view. |
|
Relevant Modes |
All modes |
Parameters |
|
<numeric> |
Choose from: 0 to 40 number of satellites to display This command accepts MIN and MAX to set the minimum power required. |
Examples |
SYST:GPS:AVER:TOPN 27 'sets the top number of satellites to be displayed at 27 SYST:GPS:AVER:TOPN MAX 'sets the top number of satellites to be dislayed to be the maximum detected |
Query Syntax |
SYSTem:GPS:AVERage:TOPN? |
Return Type |
numeric |
Default |
0 |
Last modified:
01nov2019 |
Added to PAA |
20-Jul-2010 |
New command (A.05.33) |