SYSTem:GPS:CNOise?

This query returns a string containing Carrier to Noise (C/No dBHz) data for each satellite currently in view of the FieldFox GPS.     

Note: The C/No values returned are not calibrated at the factory or warranted for accuracy. The numbers retrieved are passed unprocessed directly from the GPS receiver in use.

Relevant Modes

All modes

Examples

SYSTem:GPS:CNOise

Query Syntax

SYSTem:GPS:CNOise?

Return Type

Comma separated string in the form "sat#,cno,sat#,cno,...". If GPS mode is not enabled or there are no satellites in view, the query returns "0,0". If there are 10 satellites in view, this query generates 20 numbers in the SCPI return string.

Default

Not applicable


Last modified:

01oct2019

Added for PAA Mode