(Read-Write) Set and query the type of satellite being measured (GPS, GLNASS, BDS, GALILEO). |
|
Relevant Modes |
ALL |
Parameters |
|
<character> |
Choose from: GPS - Selects type GPS satellites to display. GLONASS or GLO - Selects type GLONASS as the satellites to display. BDS - Selects type BDS as the satellites to display. GALILEO or GAL - Selects type GALILEO as the satellites to display. |
Examples |
SYST:GPS:GNSS GLONASS 'Sets GLONASS as the only satellites to be displayed. SYST:GPS:GNSS GLO 'Sets GLONASS as the only satellites to be displayed. SYST:GPS:GNSS BDS 'Sets BDS as the only satellites to be displayed. |
Query Syntax |
SYST:GPS:GNSS? |
Return Type |
Character |
Default |
GPS |
Last Modified:
01dec2019 |
New command |