|
(Read-Write) Sets the holdoff time between triggers. When the trigger condition is satisfied, the trigger occurs, the delay begins, and the holdoff time begins. New trigger conditions will be ignored until the holdoff time expires. |
|
|
Relevant Modes |
RTSA |
|
Parameters |
|
|
<numl> |
Range: 0 seconds (0.000000E+00) to 10 seconds (1.0000000E+01) |
|
Examples |
TRIG:HOLD 1.6 ms |
|
Query Syntax |
TRIG:HOLD? |
|
Return Type |
numeric |
|
Default |
0.000000E+00 |
Last Modified:
|
20-sep-2016 |
Added new RTSA command (A.09.50). |