:TRIGger[:SEQuence]:RFBurst:DELay <num>

(Read-Write) Set and query the IQA delay for RF Burst triggers. An incoming signal with this amplitude will initiate an acquisition.

See also TRIG:RFB:DEL:STAT.

Relevant Modes

IQA

Parameters

 

<numeric>

Minimum: -150 ms

Maximum: 500 ms

Examples

TRIG:RFB:DEL 500e-3

Query Syntax

TRIG:RFB:DEL?

Return Type

Numeric

Default

0.0000000E+00 s


Last Modified:

22-Oct-2017

Added new IQA mode command (10.1x).