:TRIGger[:SEQuence]:RFBurst:LEVel

(Read-Write) Set and query the IQA trigger level for RFBurst. Similar to a Video trigger where an acquisition is triggered from a signal at the SA RF Input connector. But, an RF Burst trigger is detected in the third IF stage. An acquisition is triggered when the amplitude of the incoming signal exceeds the settable Trigger Level.  

Note: Only valid for RFBurst triggers.

Relevant Modes

IQA

Parameters

 

<numeric>

RF Burst trigger level (dBm).

Minimum: -210 dBm

Maximum: 30 dBm

Examples

TRIG:RFB:LEV -10

Query Syntax

:TRIG:VID:LEV?

:TRIG:RFB:LEV?

Return Type

numeric

Default

-25 dBm


Last Modified:

22-Oct-2017

New IQA command (A.10.1x)