:TRIGger[:SEQuence]:RFBurst:SLOPe

(Read-Write) Set and query the IQA trigger slope. Trigger Slope determines which edge of a trigger signal initiates an acquisition.

Note: Only valid for VIDeo, EXTernal, and RFBurst triggers.

Relevant Modes

IQA

Parameters

 

<character>

Trigger slope. Choose from:

POS  - Sweep is triggered by the rising (positive) edge of signal.

NEG  - Sweep is triggered by the falling (negative) edge of signal.

Examples

TRIG:RFB:SLOP NEG

Query Syntax

TRIGger:RFBurst:SLOPe?

Return Type

Character

Default

POS


Last Modified:

22-Oct-2017

Added new command for IQA mode (10.1x)