:TRIGger[:SEQuence]:VIDeo:LEVel <num>

(Read-Write) Set and query the IQA trigger level for VIDeo. An acquisition is triggered on a signal at the SA RF Input connector when the amplitude of the incoming signal exceeds the settable Trigger Level.

Note: Only valid for VIDeo triggers.

Relevant Modes

IQA

Parameters

 

<numeric>

Video trigger level (dBm).

Minimum: -210 dBm

Maximum: 30 dBm

Examples

TRIG:VID:LEV 3

TRIG:RFB:LEV -10

Query Syntax

:TRIG:VID:LEV?

Return Type

numeric

Default

-25 dBm


Last Modified:

22-Oct-2017

New IQA command (A.10.1x)