Making Waveguide Measurements

Table of Contents

The FieldFox is capable of making accurate measurements using waveguide media. Waveguide can be thought of as a bandpass filter. Waveguide is intended to pass frequencies for which it is designed and reject frequencies outside of the band.  This web site includes a table of valid frequency ranges for types of waveguide: http://en.wikipedia.org/wiki/Waveguide_(electromagnetism)

The following are tips for making good waveguide measurements in NA mode and CAT mode.

NA Mode

When using Time Domain Transform (Option 010), set transform mode to Band Pass.  Do NOT use Low Pass Step or Low Pass Impulse. These modes will attempt to set the stimulus frequencies outside the valid frequency range of the waveguide.

CAT Mode

Waveguide is limited to narrow frequency ranges of operation. When making DTF measurements in waveguide:

  1. Set Frequency Mode to [BandPass].   Do not use [Lowpass] for DTF waveguide measurements.

  2. Set DTF Min Start Frequency to the lower limit of the waveguide frequency band (also known as the cutoff frequency)   Example:  For X-band waveguide, set the Start Frequency to 8.2 GHz.

  3. Set DTF Max Stop frequency to the upper limit of the waveguide frequency band.  For X-band waveguide, set the Stop Frequency to 12.4 GHz.

Calibration