Go to description Go to description Go to description Go to description

Analyzer Calibration Measurement

Calibrate Point/Stop Calibration

Runs a single pass of the calibration operation using the frequency, bandwidth, source amplitude and analyzer input range data defined in the Calibration Points Data Table.

Calibration Points Data Table

Displays the calibration points defined in the Calibration Wizard Setup. You cannot add or delete points in this step, but you can change the frequency, bandwidth, and analyzer input range of the selected point during a continuous calibration measurement (Start Preview).

Start/Stop Preview

Starts and stops a continuous calibration. Continuous calibration allows you to change the frequency, bandwidth, and analyzer input range of the selected point to check for spurs or overlapping conditions between comb calibrator and LO frequency bands by making adjustments to point frequencies, etc.

Pass Threshold

Sets the pass/fail threshold for the calibration's magnitude mean channel response.

Calibration Settings

Contains the same Analyzer Calibration Settings that were in the Calibration Wizard Setup dialog. It may be useful to adjust these settings during continuous calibration to optimize the calibration.

Calibration Results (Graphs)

Displays the signal's magnitude and phase mean channel response and alias detection spectrum.