Open topic with navigation
Device Under Test
The Device Under Test resource block represents the user device that will be inserted into the measurement system after the source and analyzer hardware have been calibrated. The Signal Optimizer does not control the Device Under Test, so there are no Advanced or Favorite Settings. For best results, configure the source and analyzer hardware for your device before calibration, then insert your device after calibration.