This topic describes the Signal Optimizer's default Favorite Settings for the Custom IQ measurement format.
Enter the name of the resource block.
Enter a description of this measurement.
When enabled (default state), this parameter conveniently couples the measurement definition to the Selected Signal. Coupled parameters may update when Download All Signals or Run Acquisition executed. This parameter is available under Advanced for all measurement types. It does not appear under Favorites unless manually added.
Select the signal definition to be applied when Signal Coupling is enabled. This parameter is available under Advanced for all measurement types. It does not appear under Favorites unless manually added.
Enable or disable coupling of Measurement Center Frequency and Measurement Span to Analyzer Hardware Center Frequency and Analyzer Span.
Enter offset to apply to automatically determined measurement Center Frequency setting when Frequency Coupling is enabled.
Enter scale factor to apply to automatically determined measurement frequency span setting when Frequency Coupling is enabled.
Enter measurement center frequency when Frequency Coupling is disabled. When Frequency Coupling is enabled, measurement center frequency is automatically determined by Analyzer Hardware Center Frequency and Center Frequency Offset settings.
Enter measurement frequency span (bandwidth) when Frequency Coupling is disabled. When Frequency Coupling is enabled, measurement span is automatically determined by Analyzer Hardware Span and Span Scale Factor settings.
Enable automatic adjustment of Frequency Step value.
Displays the measurement resolution bandwidth (RBW).
Displays the number of unaliased frequency points to display. Should be set to p2/1.28 + 1, where p2 is a power of 2.
Enable automatic adjustment of Frequency Points value to allow for a wider range of Resolution Bandwidths (and therefore time record lengths).
Enter the filter alpha (for Raised cosine or Root Raised Cosine filters) or filter BT (bandwidth-time product, for Gaussian filters).
Enable the analyzer to search for a pulse (using the RF envelope) to determine the start of demodulation.
Select the filter applied to the measured input data during demodulation.
Choices: None| Rectangular | Root Raised Cosine | Gaussian | Low Pass
Select the filter applied to the reference data during demodulation.
Choices: Rectangular | Raised Cosine | Root Raised Cosine | Gaussian | Half Sine
Enter the number of symbols to be processed during demodulation.
Enter the amount of data over which a search is performed when Pulse Search is enabled.
Enter the expected symbol rate of the input signal.
Enter the measurement main time length.