Glossary

The following entries are defined in terms of material measurements with the N1500A software.

absorption

to take in electromagnetic energy, usually as heat.

absorption bands

distinct frequency bands at which electromagnetic energy is strongly coupled into a material and absorbed.

AC loss

dielectric loss (as D for capacitors, but excluding DC “leakage”).

Cole-Cole plot

data format, with ε " on vertical axis and ε ’ on horizontal axis, with frequency as the independent parameter not displayed; lossy materials with relaxation mechanisms follow a semi-circle on these plots.

conductivity

usually ionic dielectric loss; in dielectric measurements, does not mean true conduction (movement of electrons).

D

dissipation factor; usually measured for capacitors; D = tan δ .

Debye functions

Simplified model to explain dielectric properties versus frequency, assuming that a simple rotational relaxation phenomenon is acting.

δ

angle Delta formed between the x-axis and the permittivity vector; δ is small (nearly 0 °rees; for low-loss materials, and large (up to about 45 ° ) for lossy materials; see tan δ (used more often)

dielectric after-effect

polarization in a material lags behind the applied field in time; modeled by relaxation process; related to losses

dielectric constant

Κ ratio of electric field storage capacity in a material to that of free space; usually means real (lossless) case only.

dielectric loss

energy lost (absorbed) in material when applying an AC electric field; may be due to ionic, polar, atomic, or electronic mechanisms

dipolar

dielectric mechanism; see “rotational”

dipole

a structure where the net charge distribution can be represented by the two equal and opposite charges separated by distance

dispersion

propagation characteristics change with frequency

dissipation factor

D; ratio of energy lost to energy stored (per cycle) in a system; same as tan δ , inverse of Q.

Electronic

Dielectric mechanism (resonant, very weak, at very high frequencies), where the “orbits” of electrons around a nucleus are stretched”

ε

Epsilon, symbol for absolute permittivity; sometimes also refers to permittivity relative to free space when the subscript r is dropped.

ε r

symbol for permittivity relative to free space, also called relative permittivity. It is a complex number, ε r* = ε r' - j ε r".

free water

water molecules which are not “bound” and are free to orient themselves in an electric field

Homogeneous

having uniform properties throughout; non-homogeneous materials are usually mixtures of two or more materials.

induced dipoles

temporary dipoles, created by electric fields

ionic

a dielectric mechanism (fairly strong, lossy, operating at all frequencies), where mobile ionic charges migrate in a material

isotropic

properties do not vary with orientation; non-isotropic materials are usually fibrous or crystalline

Κ

Kappa, another symbol for permittivity, always relative to free space. If complex, Κ r * = Κ r ' - j Κ r ". Sometimes refers just to the real part of permittivity.

loss angle

see δ

loss factor

The imaginary part of permittivity ε r" or Κ r " .

loss index

The imaginary part of permittivity ε r" or Κ r "

loss tangent

another term for tan δ and Dissipation Factor

MUT

Material Under Test

NDE

Non-Destructive Evaluation

non-destructive

attribute of test method, when material can be used for its end-purpose after testing.

penetration depth

distance through a lossy dielectric over which the field strength falls by 1/e due to energy absorption

permanent dipoles

molecular structures that inherently have a non-symmetrical charge distribution

permeability (µ)

measure of effect a material has on magnetic fields; ratio of flux over field.

permittivity (ε)

measure of effect a material has on electric fields; ratio of flux over field

phase angle

see θ

phase defect angle

see δ

polar

having permanent electric dipoles

polarize

to align dipoles in electric field

power factor

sin δ (or cos θ)

Q

quality factor

Quality factor

ratio of energy stored over the energy lost (per cycle) in a system, inverse of tan δ and D

relative permittivity

permittivity relative to free space. see ε r

relaxation constant

see τ

relaxation time

see τ

relaxation wavelength

free-space wavelength corresponding to the frequency 1/ τ

restricted mobility dipoles

dipoles (such as H2O molecules) which are bound to a host material, and so are restricted in their ability to become oriented in an electric field

rotational

a dielectric mechanism (relaxation, fairly strong, often lossy, at moderate frequencies), where permanent dipoles (often entire molecules) “rotate” to align with an electric field

susceptor

material that can respond to electromagnetic fields

tan δ

ratio of ε r" over ε r'. Indicates relative lossiness of material

τ

relaxation time constant; for a simple substance, the time it takes for 1/e of the constituent molecules to become aligned in response to an electric field

δ

angle between real-axis and vector representing sum of storage and loss vectors