The Measure menu allows you to start a measurement and change the stimulus.

Note: Beginning with PLTS release 3.0, Continuous Sweep is no longer supported.
Start begins a measurement when it is selected.
Stimulus opens the Modify Time and Frequency Parameters dialog box so that you can change the parameters. For detailed information regarding changing the stimulus parameters, refer to the stimulus information of the "Setting Up the Calibration and Measurement Parameters" section in the "Setting Up and Making Measurements.