This Visual Basic program characterizes two fixture files from one 2x thru file.
|
Public Function Example_AFR() As Boolean 'create PLTS application Dim app = New PLTS.CPLTSApplication() System.Threading.Thread.Sleep(1000) 'grace time for PLTS startup app.ShowWindow(3) 'character 4-port fixtures using a 4-port 2x thru Dim xmlSettings As XElement = _ <AfrApiArgs> <Thru filePath="C:\2xThru.s4p"/> <FixtureA1 filePath="C:\fix_1.s4p"/> <FixtureB1 filePath="C:\fix_2.s4p"/> </AfrApiArgs> app.Afr(xmlSettings.ToString()) 'exit app.CloseAllFiles() app.Exit() Return True End Function |