This Visual Basic program does the following:
Loads data and opens analysis view.
Gets the number of plots.
Exports each plot to a picture file.
Gets the plot titles.
Gets the pass/fail status.
Gets the measurements in each plot.
Gets the x-axis values.
Gets the trace names.
Gets the y-axis values.
|
Public Function Example_LoadDataAnalysis() As Boolean 'create PLTS application Dim app = New PLTS.CPLTSApplication() System.Threading.Thread.Sleep(1000) 'grace time for PLTS startup app.ShowWindow(3) 'load a data and open an analysisview Dim dataFilePath As String = "C:\[DEMO] E8364B 12-port 10MHz-20GHz.s12p" Dim templateViewName As String = "USB3.0 Connector (12p)" 'case sensitive Dim docObj As Object = Nothing Dim viewObj As Object = Nothing app.ImportData(dataFilePath, templateViewName, docObj, viewObj) 'look into each plot Dim view As PLTS.IPLTSView = viewObj Dim plotsCnt As Short = 0 view.GetNumberOfPlots(plotsCnt) For i As Short = 0 To plotsCnt 'export each plot to a picture file Dim outputPicFilePath As String = "C:\plot" & i & ".jpg" view.ExportPlot(i, outputPicFilePath, 800, 600) 'get plot title Dim title As String = "" view.GetPlotTitle(i, title) Console.WriteLine(title) 'get pass/fail status Dim pass As Boolean = True Dim passFailDetails As String = "" view.GetPlotPassFail(i, pass, passFailDetails) Console.WriteLine(passFailDetails) 'get plot measurement Dim measDetails As String = "" view.GetPlotMeasurements(i, measDetails) 'get x-axis values Dim xdatObj As Object = Nothing Dim xunit As String = "" view.GetPlotTraceXData(i, xdatObj, xunit) Dim xdat As Double() = xdatObj If xdat Is Nothing Then Continue For End If Console.WriteLine("x data length: " & xdat.Length) 'get traces Dim tracesCnt As Short = 0 view.GetPlotNumberOfTraces(i, tracesCnt) For j As Short = 0 To tracesCnt 'get trace name Dim trName As String = "" view.GetPlotTraceName(i, j, trName) 'get y-axis data Dim ydatObj As Object = Nothing Dim yunit As String = "" view.GetPlotTraceYData(i, j, ydatObj, yunit) Dim trDat As Double() = ydatObj If trDat Is Nothing Then Continue For End If Console.WriteLine("trace " & j & " data length: " & trDat.Length) Next j Next i 'exit app.CloseAllFiles() app.Exit() Return True End Function |