This Visual Basic program does the following:
Sets user preferences.
Configures the measurement settings.
Gets the data from the PLTS, modifies the data, then sends data back to the PLTS.
Opens a template view.
Exports the data.
|
Public Function Example_Measure() As Boolean 'create PLTS application Dim app = New PLTS.CPLTSApplication() System.Threading.Thread.Sleep(1000) 'grace time for PLTS startup app.ShowWindow(3) 'overwrite checkbox status in 'Measure' button dropdown menu Dim xmlUserPref As XElement = _ <UserPreferencesApiArgs> <DoNotShowConnectDutWzdPg>true</DoNotShowConnectDutWzdPg> <DoNotShowSelectViewWzdPg>true</DoNotShowSelectViewWzdPg> </UserPreferencesApiArgs> app.SetUserPreferences(xmlUserPref.ToString()) '!NOTE! ATE software should call PNA API directly to setup measurement 'then call PLTS API to do sweep and pull data from PNA to PLTS Dim xmlMeasSettings As XElement = _ <MeasurementSettings> <WizardWorkMode>NewMeas</WizardWorkMode> <CalAction>LoadCal</CalAction> <SelectedAnalysisViewName>Create New</SelectedAnalysisViewName> <NumOfSweepPoints>201</NumOfSweepPoints> <VelocityFactor>1</VelocityFactor> <AverageFactor>1</AverageFactor> <IFBandWidthKHz>30</IFBandWidthKHz> <IsLogSweep>false</IsLogSweep> <CalSetName>nameOfMyCal</CalSetName> <CalDateTime>11/04/2015 09:29:27.320</CalDateTime> <NumOfDutPort>4</NumOfDutPort> <NumOfPnaPort>4</NumOfPnaPort> <PortMap>1|1|label|2|2|label|3|3|label|4|4|label|</PortMap> <DiffPortMap>1|2P|2|2P|0|UC|0|UC|</DiffPortMap> <Description>Default 4-Port Configuration</Description> <VnaPortsList>1,2,3,4</VnaPortsList> </MeasurementSettings> Dim docObj As Object = Nothing Dim viewObj As Object = Nothing app.Measure(xmlMeasSettings.ToString(), docObj, viewObj) Dim doc As PLTS.IPLTSDocument = docObj 'get data from PLTS, modify data, then set data back to PLTS Dim xmlGetDatSettings As XElement = _ <DataAccessApiArgs> <DataAccessPoint>1</DataAccessPoint> <ParameterName>SDD21</ParameterName> </DataAccessApiArgs> Dim datObj As Object = Nothing doc.GetData(xmlGetDatSettings.ToString(), datObj) Dim dat As Double() = datObj If dat IsNot Nothing Then 'modify data, for example, here change all real part to be 1, all imag part to be 0 Dim i As Integer = 0 While i < dat.Length dat(i) = 1.0 i = i + 1 dat(i) = 0.0 i = i + 1 End While Dim xmlSetDatSettings As XElement = _ <DataAccessApiArgs> <DataAccessPoint>1</DataAccessPoint> <ParameterName>SDD21</ParameterName> </DataAccessApiArgs> doc.SetData(xmlSetDatSettings.ToString(), datObj) End If 'open a template view, view name is case sensitive 'and the template view should be pre-defined Dim viewName As String = "MyDataView (4p)" Dim viewObj2 As Object = Nothing doc.OpenTemplateView(viewName, viewObj2) 'export data Dim xmlExportSettings As XElement = _ <ExportApiArgs> <FDYDataFormat>RI</FDYDataFormat> <ExportFileName>C:\pltsApi.s4p</ExportFileName> </ExportApiArgs> doc.Export(xmlExportSettings.ToString()) 'exit app.CloseAllFiles() app.Exit() Return True End Function |