Read-only |
|
Description |
Returns the last error from the error buffer. If the API return value is NOT equal to S_OK, call this method to get the detailed error information. |
VB Syntax |
plts.GetLastError errorInfo |
Variable |
(Type) - Description |
|
plts |
(object) - A PLTSApplication object |
|
errorInfo |
(String) Variable to store the returned error information. |
Return Type |
String |
Default |
None |
Examples |
Dm errorInfo |
C++ Syntax |
HRESULT GetLastError(BSTR* errInfo); |
Interface |
IPLTSApplication |