Write-only |
Description |
Show or hide PLTS main window. |
VB Syntax |
plts.ShowWindow CmdShow |
Variable |
(Type) - Description |
|
plts |
(object) - A PLTSApplication object |
|
CmdShow |
(Short) Choose from the following: 0 - SW_HIDE Hides this window and passes activation to another window. 1 - SW_SHOWNORMAL Activates and displays the window. If the window is minimized or maximized, Windows restores it to its original size and position. 2 - SW_SHOWMINIMIZED Activates the window and displays it as an icon. 3 - SW_SHOWMAXIMIZED Activates the window and displays it as a maximized window. 4 - SW_SHOWNOACTIVATE Displays the window in its most recent size and position. The window that is currently active remains active. 5 - SW_SHOW Activates the window and displays it in its current size and position. 6 - SW_MINIMIZE Minimizes the window and activates the top-level window in the system's list. 7 - SW_SHOWMINNOACTIVE Displays the window as an icon. The window that is currently active remains active. 8 - SW_SHOWNA Displays the window in its current state. The window that is currently active remains active. 9 - SW_RESTORE Activates and displays the window. If the window is minimized or maximized, Windows restores it to its original size and position. |
Return Type |
None |
Default |
SW_SHOWMAXIMIZED |
Examples |
plts.ShowWindow SW_SHOWMAXIMIZED |
C++ Syntax |
HRESULT ShowWindow(SHORT nCmdShow); |
Interface |
IPLTSApplication |