:AFR:FILE<fnum>:CORRection:PORT<pnum>[:STATe] <bool>

(Read-Write)

Set port to apply or undo AFR correction for the selected file.

Parameters

 

<fnum>

Index of the selected file.

<pnum>

Index of port for the selected file.

<bool>

Choose from:

ON (or 1) - Apply correction to the  port.

OFF (or 0) - No correction to the port.

Examples

:AFR:FILE1:CORRection:PORT1 0

Query Syntax

:AFR:FILE<fnum>:CORRection:PORT<pnum>[:STATe]?

Return Type

Boolean

Default

ON or 1