:AFR:FIXTure:USE:THRUs:SWAP <bool>

(Read-Write)

Specifies whether swapping fixtures in the latter half test channels in the multi-port configuration.

Parameters

 

<bool>

Choose from:

ON (or 1) - Swap fixtures.

OFF (or 0) - Do not swap fixtures.

Examples

:AFR:FIXTure:USE:THRUs:SWAP ON

Query Syntax

:AFR:FIXTure:USE:THRUs:SWAP?

Return Type

Boolean (1 = ON, 0 = OFF)

Default

OFF