:AFR:STANdard:NPORt:USE <fixSelect>, <fixNum>, <stanType>, <isOn>

(Read-Write)

This command chooses the calibration standards for the multi-port configuration.

Parameters

 

<fixSelect>

Selected fixture. Choose from:

        AFIXture - Fixture A.

        BFIXture - Fixture B.

<fixNum>

Fixture numbers from 1 to 32.

<stanType>

Standard Types: OPEN, SHORt or THRU.

<isOn>

ON or OFF. It indicates whether this standard will be used by AFR calculation.

Examples

:AFR:STAN:NPORt:USE BFIXture, 1, OPEN, ON

Query Syntax

:AFR:STANdard:NPORt:USE? <fixSelect>, <fixNum>, <stanType>

Return Type

Boolean

Default

OFF