|
(Read-Write) This command sets the byte order used for GPIB data transfer. Some computers read data from the analyzer in the reverse order. This command is only implemented if FORMAT:DATA is set to REAL. If FORMAT:DATA is set to ASCII, the swapped command is ignored. |
||
|
Parameters |
|
|
|
<char> |
Choose from: NORMal - Use when your controller is anything other than an IBM compatible computer. SWAPped - Use for IBM compatible computers. Note: Use NORMal if you are using VEE, Labview, or T&M Tool kit. |
|
|
Examples |
:FORMat:BORDer SWAPped |
|
|
Query Syntax |
:FORMat:BORDer? |
|
|
Return Type |
Character |
|
|
Default |
NORMal |
|