(Write-only) This command sets the reference value for delay measurement. The unit of reference value can be percent or mv, depending on the reference type, which is set by the command FILE:VIEW:PLOT:MEASure:DELay:REFerence:TYPE. |
![]() |
|
|---|---|---|
Parameters |
|
|
<fnum> |
Index of the selected file. |
|
<vnum> |
Index of the selected view. |
|
<pnum> |
Index of the selected plot. |
|
<num> |
The reference value in percent or mV. |
|
Examples |
:FILE1:VIEW1:PLOT1:MEASure:DELay:REFerence:VALue 50.0 |
|
Return Type |
Not Applicable |
|
Default |
Not Applicable |
|