(Read-Write) Sets or gets the maximum limit value of the delay measurement. Note: The command FILE:VIEW:PLOT:MEASure:DELay:LIMit:STATe ON must be sent after this command to make the maximum limit effective. |
![]() |
|
|---|---|---|
Parameters |
|
|
<fnum> |
Index of the selected file. |
|
<vnum> |
Index of the selected view. |
|
<pnum> |
Index of the selected plot. |
|
<num> |
The maximum value for delay limit. |
|
Examples |
:FILE1:VIEW1:PLOT1:MEASure:DELay:LIMit:MAXimum 10.0 |
|
Query Syntax |
:FILE1:VIEW1:PLOT1:MEASure:DELay:LIMit:MAXimum? |
|
Return Type |
Numeric |
|
Default |
10.0 |
|