:EYE:ENHanced:CONFigure:TX:PORT

(Write-only) This command sets the port number of TX.

Parameters

 

<num>

Port number of TX

Examples

:EYE:ENHanced:CONFigure:TX:PORT 1

Return Type

Not Applicable

Default

Not Applicable