|
(Read-Write) Sets the marker's X-axis value (frequency in MHz, time in ns, or distance in cm). |
![]() |
|
|---|---|---|
|
Parameters |
|
|
|
<fnum> |
Index of the selected file. |
|
|
<vnum> |
Index of the selected view. |
|
|
<pnum> |
Index of the selected plot. |
|
|
<mkr> |
Id of the selected marker. Choose from 1 to 9. If unspecified, value is set to 1. |
|
|
<num> |
Any X-axis position within the measurement span of the marker. Note: If the specified variable is out of the allowable setup range, the minimum value (if the lower limit of the range is not reached) or the maximum value (if the upper limit of the range is exceeded) is set. This command will accept MIN or MAX instead of a numeric parameter. |
|
|
Examples |
:FILE1:VIEW1:PLOT1:MARKer1:X 100MHz :FILE1:VIEW1:PLOT1:MARKer1:X MAX |
|
|
Query Syntax |
:FILE1:VIEW1:PLOT1:MARKer1:X? |
|
|
Return Type |
Numeric |
|
|
Default |
Not Applicable |
|