(Write-only) Uses a marker to search a trace for the minimum, maximum, or target y-axis value with a specified unit. If the marker search is for a target y-axis value, use one of the following units: mV, V, dB, mU, U, deg, kdeg, ns, Ohms, Ohms/M, H/M, pF/M, mS/M, Np/M, Rad/M. |
![]() |
|
|---|---|---|
Parameters |
|
|
<fnum> |
Index of the selected file. |
|
<vnum> |
Index of the selected view. |
|
<pnum> |
Index of the selected plot. |
|
<tnum> |
Index of the selected trace. |
|
<mkr> |
Id of the selected marker. Choose from 1 to 9. If unspecified, value is set to 1. |
|
<num> |
Any X-axis position within the measurement span of the marker. Note: If the specified variable is out of the allowable setup range, the minimum value (if the lower limit of the range is not reached) or the maximum value (if the upper limit of the range is exceeded) is set. This command will accept MIN or MAX instead of a numeric parameter. |
|
Examples |
:FILE1:VIEW1:PLOT1:TRACe1:MARKer1:SEARch 10dB :FILE1:VIEW1:PLOT1:TRACe1:MARKer1:SEARch MAX |
|
Return Type |
Not Applicable |
|
Default |
Not Applicable |
|