:FILE<fnum>:VIEW<vnum>:LIMit:SAVE <filePath>

(Write-only) Saves the limit test results of all plots in a view to a .txt file.

Parameters

 

<fnum>

Index of the selected file. If unspecified, <fnum> is set to 1.

<vnum>

Index of the selected view. If unspecified, <vnum> is set to 1.

<filePath>

The full path of the text file.

Example

:FILE1:VIEW1:LIMit:SAVE 'C\\sample.txt'

Query Syntax

Not Applicable

Default

Not Applicable