(Write-only) Saves the time-domain measurement data of all plots in a view to a .txt file. |
|
Parameters |
|
<fnum> |
Index of the selected file. If unspecified, <fnum> is set to 1. |
<vnum> |
Index of the selected view. If unspecified, <vnum> is set to 1. |
<filePath> |
The full path of the text file. |
Example |
:FILE1:VIEW1:TDOMain:MEASurement:SAVE 'C\\sample.txt' |
Query Syntax |
Not Applicable |
Default |
Not Applicable |