Click Utilities then Continuity Check
You can also enter Dielectric Constant or Velocity Factor from the VNA Setup Hardware dialog.
|
Set Velocity Factor dialog box help |
|
Velocity Factor - The numerical value related to the speed of energy through a DUT based on the DUTs dielectric material. Some velocity factor (Vf) examples are:
Dielectric Constant - (er) is used to calculate the velocity factor |