A "Hot TDR" measurement is performed on your data source by making a T22, TC22, or TDD22 measurement while your data source is sending a specified Bit Pattern length at a specified rate. The Hot TDR measurement dialog ensures that the VNA source and receiver is at frequencies other than those of the data source.

Click File, then New Measurement and Next>, then Perform a New Calibration.
At the Setup Hardware dialog, click BASIC/ Advanced, then click Setup Hot TDR
Calculate Hot TDR Measurement Frequencies dialog box |
In the above image:
The VNA measurement frequencies (red bars) must be more that 10 times the IF Bandwidth from the NRZ frequencies (black bars) in order to make a valid measurement. Adjust the IF BW on the Setup Hardware dialog.
1. Calculate Spectral content of the NRZ Patterns.
2. Preview: The suggested frequencies of the TDR measurement. These frequencies may be outside the range of the VNA. Adjust the frequencies as necessary in step 3. 3. Adjust Frequencies - Enter new frequencies, then click Calculate. Beginning with PLTS2022, the frequency range is limited to the frequency range of the instrument. An error message is displayed if the frequency is out side the frequency of the instrument as shown below.
|