TRL and LRM Calibration


To perform a TRL / LRM calibration:

Select TRL or LRM as the Cal Type at the Define Cal Settings dialog in the Cal and Measurement Wizard.

TRL Overview

TRL (Thru, Reflect, Line) represents a family of calibration techniques that measure two transmission standards and one reflection standard to determine the 2-port 12-term error coefficients. For example, TRM (Thru, Reflect, Match), LRL (Line, Reflect, Line), LRM (Line, Reflect, Match) are all included in this family.

The traditional SOLT calibration measures one transmission standard (T) and three reflection standards (SOL) to determine the same error coefficients.

TRL calibration is extremely accurate, in some cases more accurate than an SOLT cal. However, very few calibration kits contain TRL standards. TRL calibration is most often performed when you require a high level of accuracy and do not have calibration standards in the same connector type as your DUT. This is usually the case when using test fixtures, or making on-wafer measurements with probes.

The DUT must be physically connected to the PLTS by some kind of transition network or fixture. Therefore, in some cases you must fabricate and characterize standards in the same media type as your DUT configuration. It is easier to manufacture and characterize three TRL standards than the four SOLT standards. A limitation for TRL cal with broad frequency coverage is the requirement for multiple LINE standards. For example, a span from 2 GHz to 26 GHz requires two line standards. Also, for lower frequencies, the LINE standard can be too long for practical use.

TRL Calibration Kits

Keysight Technologies offers two cal kits that include the required standards to perform a TRL calibration: 85050C (APC 7mm) and 85052C (3.5mm). Both kits include the traditional Short, Open, and Load standards. (The Thru standard, not actually supplied, assumes a zero-length Thru). In addition, the kits include an airline which is used as the LINE standard. To use the airline, the kits include an airline body, center conductor, and insertion/extraction tools.

TRL Calibration Standards

These standards must be defined in your TRL cal kit:

THRU

REFLECT

LINE

The LINE standard establishes the reference impedance for the measurement after the calibration is completed. TRL calibration is limited by the following restrictions of the LINE standard: