This Visual Basic program:
Initializes the PNA objects.
Performs a complete ECAL confidence check
Before using this code:
The active channel must contain an S11 measurement with a 1-port or N-port calibration
Note: A confidence check can NOT be performed remotely from User Characterizations that are stored on the PNA disk.
|
Private oPNA As AgilentPNA835x.Application Private oChan As Channel Private oCal As Calibrator Private oMeas As Measurement
Private Sub cmdRun_Click() Dim iMeasIndex As Integer
Set oPNA = CreateObject("AgilentPNA835x.Application", "MachineName") Set oChan = oPNA.ActiveChannel Set oCal = oChan.Calibrator
iMeasIndex = 1
' Loop through measurements until an S11 on the active channel ' is found, or the end of the measurement collection is reached. Do Set oMeas = oPNA.Measurements(iMeasIndex) If oMeas.Parameter = "S11" And _ oMeas.channelNumber = oChan.channelNumber Then Exit Do iMeasIndex = iMeasIndex + 1 If iMeasIndex > oPNA.Measurements.Count Then MsgBox "No S11 measurement found on the active channel." _ & " Create an S11 measurement, then try again." Exit Sub End If Loop
' Set up trace view so we are viewing only the data trace. oMeas.View = naData ' Acquire the S11 confidence check data from ECal Module A ' into the memory buffer. oCal.AcquireCalConfidenceCheckECALEx "S11", 1 ' Turn on trace math so the trace shows data divided by memory. ' You can be confident the S11 calibration is reasonably good if ' the displayed trace varies no more than a few tenths of a dB ' from 0 dB across the entire span. oMeas.TraceMath = naDataDivMemory End Sub
Sub cmdQuit_Click() ' Turn off trace math ' in case someone clicks Quit without having clicked Run If oMeas <> Nothing Then oMeas.TraceMath = naDataNormal ' Conclude the confidence check to set the ECal module ' back to it's idle state. If oCal <> Nothing Then oCal.DoneCalConfidenceCheckECAL ' End the program End End Sub |