This VB Script program illustrates ENR file management using COM commands.
This VBScript (*.vbs) program can be run as a macro in the PNA. To do this, copy the following code into a text editor file such as Notepad and save on the PNA hard drive as Calibrate.vbs. Learn how to setup and run the macro.
See Other COM Example Programs
|
' Sample VBS program illustrating COM commands for ENR file management.
option explicit dim pna ' application dim enr ' ENRFile object dim scpi, hostname
set pna=CreateObject("agilentpna835x.application") set scpi = pna.ScpiStringParser set enr = pna.ENRFile
' Generate data to put in ENR file Dim vdata(3) vdata(0) = 100E6 ' first frequency point vdata(1) = 14.532 ' first ENR value vdata(2) = 20E9 ' second frequency point vdata(3) = 15.731 ' second ENR value
' send data to ENRFile object enr.PutENRData(vdata)
' Set noise source serial number enr.ENRSN = "ABCD1234"
' Write ENR file to disk enr.SaveENRFile("C:/Program Files/Keysight/Network Analyzer/Documents/sample.enr")
|
The contents of the file created by this program are shown below.
[Filetype ENR]
[Version 1.0]
[Serialnumber ABCD1234]
! Frequency ENR
! Hz dB
100000000 14.53200
2e+010 15.73100